cancel
Showing results for 
Search instead for 
Did you mean: 

Memory Interfacing with STM32H753ZIT6

Rohitgupta
Associate II

Hello Team,

I  need to connect an external NAND flash with STM32H753ZIT6 controller. 

What is the maximum capacity of NAND flash that can be interfaced with the FMC controller on the STM32H753ZIT6?

 

Thanks in advance

1 REPLY 1

Didn't you already ask this?

NAND access as a block device thru a very small window. Basically as large as you want and can afford. Figure many 100s of GB.

Consider using eMMC devices

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..