cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f303zet6 custom board not working

shankarachary
Associate

Dear sir/Madam,

I have made a custom stm32f303zet6 board for my applications. I started with a basic Led blink program. program is flashing into the MCU but the led blink is not happening. Here i am attaching the schematic for the custom board. Please help me in getting the customized PCB work.

Thanks & Regards,

3 REPLIES 3
Andrew Neil
Super User

So what debugging have you done so far, and what have you learned from that?

Are you sure that the LEDs are mounted the correct way around?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
ONadr.1
Senior III

Are you using an internal oscillator for the MCU? According to the schematic, you only have a low speed oscillator crystal connected. Share your code and clock and IO settings.

mƎALLEm
ST Employee

Hello,

Are you sure you're toggling the correct LED?

Share with us your source code.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.