2024-06-06
10:58 PM
- last edited on
2024-06-07
02:34 AM
by
Lina DABASINSKAITE
Hello Team,
I need to connect an external NAND flash with STM32H753ZIT6 controller.
What is the maximum capacity of NAND flash that can be interfaced with the FMC controller on the STM32H753ZIT6?
Thanks in advance
2024-06-06 11:25 PM
Didn't you already ask this?
NAND access as a block device thru a very small window. Basically as large as you want and can afford. Figure many 100s of GB.
Consider using eMMC devices