cancel
Showing results for 
Search instead for 
Did you mean: 

MCU consulting STM32F412RGT7

Zhong
Associate

May I ask whether ST has STM32F412RGT7 model and Operating temperature to 105°C.TKS!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
STTwo-32
ST Employee

Hello @Zhong and welcome to the ST Community :smiling_face_with_smiling_eyes:.

according to the DS11139:

STTwo32_0-1702545478668.png

The MCU STM32F412RGT7 doesn't exist but we have the STM32F412RGT6 and STM32F412RGT6TR who support a temperature range between -40 to 85 °C and we have the STM32F412VGT7who support a temperature range between -40 to 105 °C.

For more details on available MCUs you can take a look on the MCU/MPU selector of the STM32CubeMX.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

waclawek.jan
Super User

You can see the available variants in the website of the base model (here STM32F412RG) under "Sample&Buy" tab.

Also, if you look at the table in "Product selector" tab of the whole series, there is a "Maximum temperature" column, so you can select according to that (e.g. there is a -7 suffixed STM32F412RE - although real availability at distributors may still be questionable).

JW