MCU Clock Frequency change
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-15 3:12 AM
Posted on January 15, 2018 at 12:12
MCU: STM32L443VCT6
Hi,
We have earlier generated code using CubeMX. After that, entire application have been developed on the generated code/project. But midway, there is a requirement of changing the clock frequency from 80 MHz to 24 MHz. Since, the application is developed almost 80%, we cannot generate the code again using the CubeMX. But instead, we need to know which parts of the code (configuration section(s)) needs to be changed to get 24 MHz CPU frequency from existing 80 MHz setting.
Can anyone point out which configuration functions need to be changed or which section of the generate code needs to be modified to cater to the CPU clock frequency change?
#cpu-clock-frequency #cpu #cubemx #stm32l4 #stm32l443
Labels:
- Labels:
-
STM32L4 Series
0 REPLIES 0