2023-10-20 1:34 AM
Hello ST Community,
i am currently working with MATLAB/Simulink and STM32 Nucleo Boards. Now i am facing a problem: I want to use "Run on Hardware Board" using "STM32L4xx Based" option in Simulink model settings. However, since i have to work offline, i cannot use for example CubeMX to download firmware packages and must get them from other sources. My problem is, that MATLAB cant find some firmware packages and wants to download them (See picture). My question is: What exact firmware packages does the installer wants to download? It only states "STM32L4xx Based MCUs". Furthermore, in which location do I have to put them? (I am working with the NUCLEO-L496ZG)
Thanks in advance,
ChRegBrg
2023-10-20 2:03 AM
Hello,
maybe i have to add, that i have the "STM32CubeL4-1.17.2" firmware package (I can build an run projects with the STM32CubeIDE).
Greetings