2025-01-08 7:21 AM
We have made a batch of 30 boards using the STM32U073. One of this 30 boards is not working as expected.
I am able to connect STM32CubeProgrammer to the processor using the SWD port. I am using STM32CubeProgrammer v2.18.0. If I try and erase the flash I get ”Error: Mass erase operation failed! Please verify flash protection”.
Using the OB – Option Bytes page I see the following.
RDP = AA
WRP1A_STRT = 0x7F
WRP1A_END = 0x0
WRP1B_STRT = 0x7F
WRP1B_END = 0x0
This looks like RDP is level 0 (no read protection) and the two write flash areas are unprotected.
I do not know if the following is related but I noticed the following while investigating this issue.
2025-01-08 8:13 AM
If 1/30 isn't working, probably more likely to be a hardware issue than a software configuration thing. The error message is telling you something went wrong but is just guessing at the cause. In any case, it seems way more likely to be a manufacturing issue with the board than for the FLASH on the chip to be programmed incorrectly.
Can you verify soldering on the chip? Verify VDD level. Is current draw the same as other boards?
2025-01-08 8:50 AM
Hi,
I would just tell to you, having experienced a such memory mass erase you should take care about which memory you want to erase. A mass erase, erase all the NVM including system memory. If you want just erase the NVM where you expect to store your application, this is the application memory, you should see in software parameters.
My own experience is making a mass erase, I loose a Nucleo board, loosing all system functioality including boot loader.
A counter solution is to erase the application memory page by page. For my own need this is an application which can be develloped through the Bootloader.
Wishing this information, can help.
Butterfly.
2025-01-08 10:35 AM
> A mass erase, erase all the NVM including system memory
This is just plain horse hockey (not true). Mass erase does not erase system memory (i.e. the built-in bootloader).
2025-01-08 11:11 AM
Hi, I'm really enjoyed with your joke.
I can testimony I did a mass erase through the boot loader, and I wasn't able to use my Nucleo board, after this mass erase.
Then, the subject of my mail was just to pay attention, which kind of memory you want to use as target. The NVM being separate between several objects, a mass erase, erase all objects.
Regards.
Butterfly.
2025-01-09 1:49 AM - edited 2025-01-09 1:50 AM
Hopefully to eliminate the question around mass erase in our case. We also have other identical cards where I have been able to perform the same erase operation without errors and it boots and runs our code as expected.
2025-01-09 3:25 AM - edited 2025-01-09 4:34 AM
Several people have visually checked the soldering.
I measured VDD on both the good and failing boards. They are both 3.29V.
My circuit is a USB device which is bus powered. I was also able to measure the USB bus current with USB32CubeProgrammer connected and it was 3.32mA on the failing board. On the good board this current was 3.35mA.
2025-01-09 6:48 AM
Hi,
The only good answer I can do for this question, is to check application software functionality.
View from the STM32, a mass erase, all the full NVM, that means the user application memory, and the system memory. In short the MCU can't run in any case.
Regards.
Butterfly.
2025-01-13 9:56 AM
Getting a bootloader version of 0xff sounds like a communication failure over SWD. What do you have connected to the SWD related signals (SWCLK, SWDIO, NRST). I'm not familiar with the U073, but also check all power pins (VBAT, VREF+, VUSB, etc.).
Were the PCBs electrically tested by the fab house? Hand assembled or automated pick-n-place?
Also, bulk erase can draw significant current - check for incorrect components in the power supply to the STM32. You might also need an oscilloscope to look for a temporary droop in the power rail.
2025-01-14 12:47 AM
Hi Bob S,
Thanks for the comments. But you seem to mixe two mcufunctionalities, boot loader and debugger. Naming of pins referring to debugger, and boot loader version referring to boot loader, and initial request referring to mass erase.
Then I am not sure what is your concern?
From the debugger point of view, this is a 2 pins interface (SDIO, SWCLK), SWCLK is input on the MCU, and SWDIO bidirectionnal. Reset is done with a particular series of clock cycles. Personnally I use a fast prototyping board to evaluate prototypes and protocols.
Regards.
Butterfly.