2019-06-06 5:05 PM
Using:
The reference manual seems to state that a Mass Erase must be performed before every FSTPG. However the requirement is not clear.
Assuming it is correct that a Mass Erase is required to use FSTPG:
1.Is there a time window after the Mass Erase that the FSTPG can be used?
2.Once FSTPG is set, can I just keep writing (successive) flash locations (while meeting 8 msec timeout in the manual)?
3.Can I de-assert FSTPG and later resume FSTPG programming in this same bank?
4.Can I use standard programming for a small block and then switch to FSTPG (on a properly aligned location)
*REALLY* hoping the requirement for FSTPG is a simple page erase and not a Mass Erase. Fingers-crossed... :)
Cheers,
+Joel.