cancel
Showing results for 
Search instead for 
Did you mean: 

Lost debug messages from LORA WAM STM32WL device

markpow
Associate III

I lost debug messages from my LoraWAN end device. I made some changes using MX on my project, and this way, I lost debug messages displayed on a serial wire monitor (for example, on Arduino serial monitor). I think it was the cause of this problem. No, I see that red and blue LEDs stopped blinking. Usually, red links when a concentrator doesn't accept a join, and blue blinks when sending messages).
I checked the settings responsible for logging and debugging, and I see that they have the right values:

markpow_0-1703241149646.png

Is there anybody who can explain how to revert my end device to its former state?

 

10 REPLIES 10

Even with this, I don't see this message in the serial port:

markpow_1-1703676503566.png