2023-12-01 1:07 PM
Hello,
I am currently working to get CAN transmission to work on a STM32F072B-DISCO. I am continuously getting a BIT_DOMINANT_ERROR in the LEC of the CAN_ESR when attempting to transmit.
I am using a TCAN1044 (https://www.ti.com/lit/ds/symlink/tcan1044v-q1.pdf) as the CAN transceiver with the following connections:
TCAN PIN | Connection
1 | PA12
2 | GND
3 | 5V
4 | PA11
5 | 3V
6 | CANL
7 | CANH
8 | GND
There is also a 120 ohm terminating resistor at both ends CAN Bus, and only one other device is connected, which is a PCAN-USB reader for viewing transmitted CAN messaged. The PCAN was tested previously on another device and works without issues.
Here is my code:
/* USER CODE BEGIN Header */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t egg[8] = {'5',0,0,0,0,0,0,0};
uint32_t TxMailbox;
CAN_TxHeaderTypeDef TxHeader;
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN_Init();
/* USER CODE BEGIN 2 */
HAL_CAN_Start(&hcan);
TxHeader.StdId = 0x056;
TxHeader.ExtId = 0x01;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
uint8_t sleepy;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while(1){
HAL_Delay(100);
HAL_CAN_AddTxMessage(&hcan, &TxHeader, egg, &TxMailbox);
HAL_Delay(10);
sleepy = HAL_CAN_IsTxMessagePending(&hcan,TxMailbox);
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief CAN Initialization Function
* @PAram None
* @retval None
*/
static void MX_CAN_Init(void)
{
/* USER CODE BEGIN CAN_Init 0 */
/* USER CODE END CAN_Init 0 */
/* USER CODE BEGIN CAN_Init 1 */
/* USER CODE END CAN_Init 1 */
hcan.Instance = CAN;
hcan.Init.Prescaler = 16;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_1TQ;
hcan.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = ENABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = DISABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
/* USER CODE END CAN_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */When viewing PA12/CAN_TX pin on an oscilloscope, the voltage remains constant when running.
When unplugging the other device, the BIT_DOMINANT_ERROR persists.
At this point, I'm not sure if it's a software or hardware issue. Would anybody be able to run this code on their own hardware that is known to work with CAN and verify if it is a hardware or software issue?
Thanks.
Solved! Go to Solution.
2023-12-05 8:38 AM - edited 2023-12-05 8:40 AM
Hello @PF-JohnF ,
At a first glance I have two remarks based on what you provide as source code:
1- It's not recommended to use HSI clock as source clock for CAN communication. As you are using STM32F072B-DISCO board, I recommend you to use The clock generated by STLink module through its MCO output and solder the solder bridge SB19 to connect MCO to PF0-OSC_IN of your MCU. You need to configure the RCC source clock in Bypass mode.
2- Your values of BS1 and BS2 are very low. You need to increase them as much as possible in order to let BS1 ~70 to 80% of the bit time. You need to decrease your CAN prescaler to match this requirement.
I've attached a zipped .ioc file for you reference.
- CAN bitrate = 1Mb/s
- SysClock = 48MHz
- External source clock = 8MHz
- CAN prescaler = 3
- BS1 = 12
- BS2 = 3
2023-12-05 8:38 AM - edited 2023-12-05 8:40 AM
Hello @PF-JohnF ,
At a first glance I have two remarks based on what you provide as source code:
1- It's not recommended to use HSI clock as source clock for CAN communication. As you are using STM32F072B-DISCO board, I recommend you to use The clock generated by STLink module through its MCO output and solder the solder bridge SB19 to connect MCO to PF0-OSC_IN of your MCU. You need to configure the RCC source clock in Bypass mode.
2- Your values of BS1 and BS2 are very low. You need to increase them as much as possible in order to let BS1 ~70 to 80% of the bit time. You need to decrease your CAN prescaler to match this requirement.
I've attached a zipped .ioc file for you reference.
- CAN bitrate = 1Mb/s
- SysClock = 48MHz
- External source clock = 8MHz
- CAN prescaler = 3
- BS1 = 12
- BS2 = 3
2023-12-26 11:19 PM
Hi @mƎALLEm I am also facing the same issue i tried modifying the clock source to HSE_BYPASS on STM32F407 discovery board. can you give me more details about how to solve this issue
2023-12-26 11:21 PM
Hi @PF-JohnF Were you able to solve the issue if Yes can you help me as i am also facing same condition. Thank you in advance
2023-12-27 5:10 AM
Depending on the port/pins you are using, you may need to connect some solder bridges on the back of the board. On the STM32F072 board, I had to solder SB20 and SB23 bridges to connect PA11 and PA12.
There may also be a solder bridge necessary to connect HSE to the microcontroller as well.