2019-06-12 12:26 PM
I have configured LPUART with 9600 baud rate and enable receiver interrupt with MCU 65Khz low power mode and my uart handler like
void LPUART1_IRQHandler(void)
{
uint32_t isrflags = READ_REG(hlpuart1.Instance->ISR);
uint32_t cr1its = READ_REG(hlpuart1.Instance->CR1);
uint32_t errorflags;
/* If no error occurs */
errorflags = (isrflags & (uint32_t)(USART_ISR_PE | USART_ISR_FE | USART_ISR_ORE | USART_ISR_NE));
if (errorflags == RESET)
{
/* UART in mode Receiver ---------------------------------------------------*/
if(((isrflags & USART_ISR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))
{
UART_RX_Buffer[UART_Buffer_Counter]=LPUART1->RDR;
UART_Buffer_Counter++;
if(UART_Buffer_Counter==UART_RX_BUFFER_LENGTH)
UART_Buffer_Counter=0;
return;
}
}
}
and 200ms sytem tick interrupt,
2019-06-12 12:36 PM
Make sure the interrupt grouping/priority is such that this routine preempts others that can run excessively. ie SysTick or others doing a whole bunch on ancillary things.
Don't do any additional processing in the handler beyond filling the buffer.
2019-06-12 1:13 PM
So the CPU is running at 65KHz. That means that you have approx 67 CPU clock cycles to respond to each UART interrupt (presuming 8-bit data, no parity which gives 960 bytes/sec). And that includes the exception setup/cleanup and stacking and unstacking registers. Going with what @Community member said, and presuming that your ISR uses fewer than that many clock cycles (it looks like it should), then that doesn't leave a whole lot of time for anything else to preempt the LPUART_IRQHandler().
2019-06-13 2:33 AM
Thank you
When UART communication only Systick interrupt enable with 200ms.