cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for a MCU with SPI interface for 24 channel LED driver only.

ECY
Associate

I am planning to use LED2472GQTR 24 channel LED driver for a project but MCU used in the EVK is STM32F103C6T6 which is a 32 bit MCU. My application is only driving LEDs nothing more. Any simple MCU with SPI interface around 20 to 28 pin count can be suggested ?

Thanks

2 REPLIES 2

What's wrong with a 32-bit micro-controller with current debug and development tools?

You have a preferred 8-bit architecture you have some existing experience with?

Could probably find a small STM32 Cortex-M0(+) part in 8 or 20 pin SOP

https://www.embedded.com/arm-cortex-m0-based-mcu-comes-in-8-pin-packages/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ECY
Associate

Thanks for the suggestion. I'll look in to it.