cancel
Showing results for 
Search instead for 
Did you mean: 

Location of HAL_ADCEx_Calibration_Start() source code

LThal
Associate III

Hi all. I'm trying to find the source code for the HAL function HAL_ADCEx_Calibration_Start(). I'm working with the STM32L152. I've downloaded the latest version of STMCube (STMCube_FW_L1_V1.9.0), and looked in stml1xx_hal_adc.c and stm32l1xx_hal_adc_ex.c, and haven't found it. 

Any chance someone could point me to where I can find it? Is this function not available for this family? Thanks.

Lee

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

The "ex" functions are functions which are specific to a given family.

Read the ADC chapter in RM - is there any mention of calibration?

JW

LThal
Associate III

There's a section on calculating actual Vdda voltage from the reference, but no mention of any calibration process. Does this mean that other families have an actual ADC calibration sequence? If so I'll just use the reference voltage calculation for Vdda.

Lee

LThal
Associate III

I was referring to the hardware family UM. I checked the HAL UM for my part, which I thought had a calibration routine, and just solved my confusion. In the UM section covering an overview of the manual API descriptions, it used the ADC calibrate routine as an example of an extended API, which I assume I found when I did a search of the manual for "calibrate". I didn't realize it was only an example. The ADC section of the manual itself does NOT have the calibrate function listed. Thanks for your response Jan.

Regards,

Lee