2011-01-21 2:41 PM
Loading multiple executables on the STM32 flash memory
2015-03-13 4:35 AM
>> 'With BIN files you'll have to make you own application/linker/loader to represent the entire flash footprint,
>> and load the respective BIN files into their assorted position within that space, and then write that consolidated BIN file back out to another file.' > This is exactly what I want to do with some binary files I've got. Rather than go and write my own application, > I was just wondering if you (or anyone else) knew of an application that's already out there that might do the job? Clive told you that already above: ''application/linker/loader'' For a simpler (but still powerful and specialized in certain ways) tool, check out srecord. JW2015-03-13 5:11 AM
There may be several general apps, you might find you have to reread the instructions every time you pick them up. As Jan mentions, srecords, is perhaps a good starting point and one that recognizes many input formats.
At a binary level I think of these as throw-away apps, something that can be coded in 5-10 minutes to perform a very specific task, I've coded hundreds of them, a lot of them historically did byte/word swapping, of byte/word splitting, to generate gold images for EPROM programmers, and run as part of the make process.Generally such a tool will use C staples like fopen/fclose/fseek/fread/fwrite, malloc/free, memset/memcpy.I've also built much more complicated solutions, that can take and output, hex and object files, and translate between formats.2015-03-13 9:49 AM
In case anyone else is interested, I managed to achieve what I was after by creating a single dfu file out of the two binaries, programmed my arm chip with the dfuse app, and then extracted the binary from the chip using the ST Link, and voila- one single binary. Does the job.
2015-06-03 2:03 PM
I'm working on combined DFU/CDC flash image and you can also just use dd to zero pad out the first bin file and then use cat to append the second bin file to create a single flash image.
jeff2015-06-03 3:29 PM
Probably, but I'd be tempted to code a small app to automate the work, basically padding out the the right size, and making sure everything fit in the right spots and is suitably checksummed.
In DOS two binary files can get concatenated with COPY /B A.BIN+B.BIN C.BIN