2013-11-20 08:39 PM
2013-11-20 11:41 PM
Add the preprocessor macro ''USE_STDPERIPH_DRIVER'' to your project settings, this should solve the problem. Not sure how to do this in the IAR WB. In a Makefile-based project, one would append ''-DUSE_STDPERIPH_DRIVER'' to the CFLAGS.
If you want to know why, look how this macro is used in stm32f4xx.h.2013-11-21 05:37 PM
I'm new with IAR I don't know how to set the make file or even where finding it :/
I was working with pic and programe them using pic c compiler and I had never have those problem of linking files.2013-11-21 05:57 PM
I solved the problem by including libarary manually in the drivers of the lis302 and the codec . but I'm having a new type of error when I defining some new function :
Error[Li006]: duplicate definitions for ''config_audio_codec''; in ''C:\Users\Amir\Documents\IAR Embedded Workbench\For discovery\STM32F4-Discovery_FW_V1.1.0\Project\Audio project\ Audio project v1\Debug\Obj\Audio_config.o'', and ''C:\Users\Amir\Documents\IAR Embedded Workbench\For discovery\STM32F4-Discovery_FW_V1.1.0\Project\Audio project\Audio project v1\ Debug\Obj\main.o'' I didn't defined that function in another file2013-11-21 06:29 PM
Here the defines used for the STM32F429I-DISCO, I prepared the art so posting it all the same.
I'm not sure it matters if you defined the function or not, it's in one of the project files, shares the same name space, and clashes with yours. So you'll either have to use a different name if it's a different function, or pick which of the instances or files you want to use.2016-08-03 11:22 PM
hi i have given the paths as shown but still i'm getting this error , please help me to solve this
Error[Pe020]: identifier ''GPIO_Pin_12'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 69 Error[Pe020]: identifier ''GPIO_Pin_13'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 69 Error[Pe020]: identifier ''GPIO_Pin_14'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 69 Error[Pe020]: identifier ''GPIO_Pin_15'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 70 Error[Pe020]: identifier ''RCC_AHB1Periph_GPIOD'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 71 Error[Pe020]: identifier ''GPIO_Pin_0'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 76 Error[Pe020]: identifier ''RCC_AHB1Periph_GPIOA'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 78 Error[Pe020]: identifier ''EXTI_Line0'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 80 Error[Pe020]: identifier ''EXTI_PortSourceGPIOA'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 82 Error[Pe020]: identifier ''EXTI_PinSource0'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 84 Error[Pe020]: identifier ''GPIO_InitTypeDef'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 118 Error[Pe020]: identifier ''GPIO_Mode_OUT'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 125 Error[Pe020]: identifier ''GPIO_OType_PP'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 126 Error[Pe020]: identifier ''GPIO_PuPd_UP'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 127 Error[Pe020]: identifier ''GPIO_Speed_50MHz'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 128 Error[Pe020]: identifier ''GPIO_InitTypeDef'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 190 Error[Pe020]: identifier ''EXTI_InitTypeDef'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 191 Error[Pe020]: identifier ''RCC_APB2Periph_SYSCFG'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 196 Error[Pe020]: identifier ''GPIO_Mode_IN'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 199 Error[Pe020]: identifier ''GPIO_PuPd_NOPULL'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 200 Error[Pe020]: identifier ''EXTI_Trigger_Rising'' is undefined D:\Ramya\STM32F4\STM32F4_Discovery Kit\STM32F4-Discovery-Firmware-master\STM32F4-Discovery-Firmware-master\Utilities\STM32F4-Discovery\stm32f4_discovery.c 2122016-08-04 02:29 AM
Have you added the define ''USE_STD_PERIPH_DRIVER'' to your project ?