2024-10-26 05:41 PM
Hello,
I have a Asus Vivobook S15 with Windows 11. I want to connect stm32f407g-disc1 + in my laptop but my laptop does not recognize the device. It is not the problem of the cable nor the device because I used them in other laptops and they get recognized. then it produces an error and does not recognize the device as part of "USB Devices". The system is updated. I tried to download a drive, a software to upgrade the device but it fails to install. I also turned off the firewall and security temporarily, but it did not work. What can I do in order to make my laptop recognize the device as usb-connected device?
thank you in advance for the help.
2024-10-28 10:58 AM
Hello @St_user3 ,
Maybe the problem is with the port of your laptop.
Did you try upgrade the ST-Link firmware version through : ST-LINK>firmware update or STSW-LINK009.
Verify that the jumpers on the board are correctly set and that the board is properly powered.
2024-10-28 11:03 AM
Things to try when the computer is not seeing the ST-Link:
@St_user3 wrote:It is not the problem of the cable nor the device because I used them in other laptops and they get recognized..
I would still suggest trying other cables - they can be marginal.
Also check the board very carefully - the connector can become loose/unreliable