cancel
Showing results for 
Search instead for 
Did you mean: 

Lan8742 Hardfault

GreenGuy
Lead

Stats:

STM32CubeIDE

Version: 1.13.2

Build: 18220_20230914_1601 (UTC)

 

Windows 10 Enterprise

 

I have a project using STM32H743 and Azure RTOS, ThreadX, NetX, and FileX.

In the NetX portion during initialization of the netx thread, the code performs initiation of the LAN8742 device.

Here is the call stack tree in the debugger:

GreenGuy_0-1695862962474.png

The hard fault occurs on line 131 in the lan8742.c code which is :

if(pObj->IO.WriteReg(pObj->DevAddr, LAN8742_BCR, LAN8742_BCR_SOFT_RESET) >= 0)

The Status registers show:

GreenGuy_1-1695863168854.png

The fault is 100% repeatable.

The fault appeared after adding some code to a completely unrelated section

and the fault happens prior to any of the added code being executed. As far as I can tell

The only difference is that the added code has pushed the LAN8742.c code a

little farther down in the flash. I also noticed that some of the printf()'s for debug also

cause issues like mem faults and have to be commented out. I am not finished experimentation

with what causes the hard fault in the Lan8742 code but any comments at this pint are welcome.

 

 

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

This is true, but in this case not much help or at least not much different than inspecting the stack and the fault registers.  But as it turns out the error always occurs on the same statement which was a strtok call.  Further research shows the strtok call to not be thread safe.  strtok_r() is and it works.  The faults are not occurring anymore.