cancel
Showing results for 
Search instead for 
Did you mean: 

Keil uv5 application hangs when I add Large C file and The only way out is "killing" uVision via Windows 10 task manager.

GR.5
Associate II

MCU: STM32L071cz

Application : MDK-ARM essentials version 5.35

 when I try to build large project. The "Build Output" window freezes at a random point in the build. uVision is still responsive but I can't stop the build or quit uVision. The only way out is "killing" uVision via Windows 10 task manager. Does anyone know the root cause for this?

1 REPLY 1
AMuya.1
Associate II

Have you been able to resolve this? I am having the same issue