2013-09-14 04:18 PM
Guys I got :
Guys, I got error on reading STM32 : What should I fix ? thanks **JLink Warning: Identified core does not match configuration. (Found: None, Configured: Cortex-M3) * JLink Info: TotalIRLen = 9, IRPrint = 0x0011 **JLink Warning: Identified core does not match configuration. (Found: None, Configured: Cortex-M3) **JLink Warning: CPU not halted after Reset, halting using Halt request ***JLink Error: Could not power up debug port: Control/Status register reads 000000F0 Is it because of my crystal not connected properly or something else ? thanks2013-09-14 07:32 PM
Is it because of my crystal not connected properly or something else ?
I'm going to go with something else. I'd check the supplies, especially the analogue one. I'd check the reset. Failing that I'd want to see a schematic about how/what is wired up where.2013-09-14 08:51 PM
2013-09-14 08:57 PM
2013-09-14 10:20 PM
is it about unlock option register with JLink commander ?
It's working allright now, after I resoldered all the pins, I think there was a dry join before, thanks for helping