2017-02-23 4:04 AM
Hello,
We are developing a PV converter and we have choose an STM32F407VGT microcontroller in order to controlling its power electronics and communications.
We are using the
♯
in order to ensuring that the software works properly and if not reset the system and initialize in a safe state. Mainly stopping the PWM modules and stop triggering the Mosfets. We would like configuring the IWDG at minimum period (125us). We carries out the IWDG reset in a timer (TIM2) update event interrupt each 50us. For reseting de WDG we are using the HAL function HAL_IWDG_Refresh(&hiwdg). Following is the IWDG initialization code:hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_4;
hiwdg.Init.Reload = 0;
if (HAL_IWDG_Init(&hiwdg) != HAL_OK)
{
Error_Handler();
}
We have tested 3 different values for hiwdg.Init.Reload, 0, 1, and 2. If we use 0 or 1 the systems restarts continuously. If we use 2 the watchdog works, but four application the watching time is too long and produce that some converter components could explode. How can we configuring the IWGD in order to having a WD period of 125us as told in the manual reference?
#iwdg #stm-32 #stm32f407 #problem2017-02-23 10:37 AM
Okay, so you clear the watchdog at 3X the required rate by doing it in a timer, and yet the system still resets.
Perhaps you should turn off the watchdog and use the timer routine to toggle an I/O pin so you can check your timing with an oscilloscope.
Your program is obviously not doing what you think it is.
2017-02-23 10:40 AM
Sorry I have just remark that in the last results, the system clock was configured at 16MHz. I am going to repeate the tests with 168MHz but I think that from the point of view of the WD I will continue need reseting it 7 times faster. Is it normal?
2017-02-23 11:08 AM
Configuring the clock at 168MHz and doing the reset as fast as possible (5,56MHz each 219ns) and with hiwdg.Init.Reload = 0, the system continuous restarting. With
hiwdg.Init.Reload = 1 the system do a restart if I do not reset the IWDG at a frequency higer than 30kHz (each 33,3us).
Any one knows if this performance is normal?
Why the manual reference (
) in the page 712 sais that minimum timeout are 0,125us if it do not work?Furthermore I have check too that the registers are right configured:
2017-02-23 11:34 AM
I have already test that the reset code is been executed. I have already monitoring with a GPIO output. As I show:
while (1)
{ HAL_GPIO_WritePin (GPIOD,GPIO_PIN_12,GPIO_PIN_SET); HAL_IWDG_Refresh(&hiwdg);HAL_GPIO_WritePin (GPIOD,GPIO_PIN_12,GPIO_PIN_RESET);}
The results are:
hiwdg.Init.Reload = 0; (teorically 125us IWDG period) Reseting continuously the whatchdog in the main (429,8 kHz or 2.326 us aprox) the system do a reset.
Fig1
Fig2
hiwdg.Init.Reload = 1; (teorically 250us IWDG period) I have the same result than in the Fig 2 but without interruption due to a reset.
In this case I have introduced a delay with a for loop:
while (1)
{HAL_GPIO_WritePin (GPIOD,GPIO_PIN_12,GPIO_PIN_SET); HAL_IWDG_Refresh(&hiwdg); for(uint32_t i = 0; i < 150; i++); HAL_GPIO_WritePin (GPIOD,GPIO_PIN_12,GPIO_PIN_RESET);}
for maintain the system working I need to do the reset the IWGD at a frequency of 29,39 kHz (each 34,02 us);
Why I need reset the WD counter 7 times faster than it runs? That is what I do not understand.
In any case I am very grateful for the help that all of you is giving to me !!!
2017-02-23 12:24 PM
What hardware do you use?
If it's a custom board:
JW
2017-02-23 3:29 PM
The timer IWDG shall be dumped in a cycle of a feedback loop of a contour of management. It is a general contour of management, its tasks include calculation of the current speed of rotation of an anchor of the engine, more precisely than its vector. The processor shall manage to execute this piece of a code till the moment when calculations are still urgent. If isn't in time - means there was an accident. Dumping of IWDG shall be program, start of an operation cycle of a feedback loop - on the timer.
Protection of power cascades is carried out at the level of simple logic, the more simply - the more reliably.
2017-02-24 12:52 AM
The last tests have been done with a STM32F407VGT evaluation board even using 2 different boards.
2017-02-24 12:53 AM
Hear is the Code wich fails I have remaked the relevant parts:
/* Includes ------------------------------------------------------------------*/
#include 'stm32f4xx_hal.h'/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
IWDG_HandleTypeDef hiwdg;/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*//* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);void Error_Handler(void);static void MX_GPIO_Init(void);static void MX_IWDG_Init(void);/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*//* USER CODE END PFP */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
int main(void)
{/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* Configure the system clock */
SystemClock_Config();/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_IWDG_Init();/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin (GPIOD,GPIO_PIN_12);
HAL_IWDG_Refresh(&hiwdg); } /* USER CODE END 3 */}
/** System Clock Configuration
*/void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.LSIState = RCC_LSI_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 4; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); }RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); }HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}/* IWDG init function */
static void MX_IWDG_Init(void){hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_4; hiwdg.Init.Reload = 0; if (HAL_IWDG_Init(&hiwdg) != HAL_OK) { Error_Handler(); }}
/** Configure pins as
* Analog * Input * Output * EVENT_OUT * EXTI*/static void MX_GPIO_Init(void){GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE();/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);/*Configure GPIO pins : PD12 PD13 PD14 PD15 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence. * @param None * @retval None */void Error_Handler(void){ /* USER CODE BEGIN Error_Handler */ /* User can add his own implementation to report the HAL error return state */ while(1) { } /* USER CODE END Error_Handler */ }#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* USER CODE END 6 */}
#endif
/**
* @} *//**
* @}*/2017-02-24 1:24 AM
More or less this is the performand of the real code. But my problem is that I can not dump the IWDG when it is configures at 125us even if no more code is excuted. Only writing the register continuousli in the main to carry out the IWDG reload.
2017-02-24 1:28 AM
Try to switch on LSI (and wait until it signals ready) before switching on IWDG.
JW