2025-08-13 4:23 PM - last edited on 2025-08-18 3:34 AM by Amel NASRI
Hello,
I hope this message finds you well. I am currently testing two MT25QL512ABB devices in dual mode using the STMH747I, with the same driver for the MT25QL512ABB. After performing write/read verification and rebooting, I encounter issues during subsequent read operations, as it consistently returns 0xFF. I would greatly appreciate your assistance in sharing any insights or findings regarding the root cause of this issue, if available. Thank you in advance for your support.
Edit: moved from Issue with Programming NOR Flash MT25QL512ABB1EW9 Using STM32H735IGT6 to a new thread.
2025-08-20 7:46 AM
Hello,
Same issue is reported here.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.