2024-04-11 12:24 PM
I began using an STM32G473 and the DAC outputs are acting funny. I have VREFBUF configured as an internal reference. Since I'm not using VREF+ as an output, I left the pin unconnected. I posted a thread about it and it was recommended that I connect VREF+ through a cap to ground. I'm working with a custom board where this isn't possible so I can't test.
I haven't found anything in the documentation that would suggest leaving the VREF+ pin unconnected would have ill effects on DAC outputs. Is this documented anywhere?
Original thread:
Solved! Go to Solution.
2024-06-21 01:00 PM
The observational data was polluted by a raft of other issues but resolved with the data in the above replies.
2024-04-11 01:13 PM - edited 2024-04-11 01:17 PM
> Is this documented anywhere?
Sure.
Importance of stable VREF+ for stable DAC is not a question, I suppose.
JW
PS. Please don't start new threads while discussing the same issue. Please select @AScha.3 's correct answer as "Accept as solution" so that the thread is marked as solved.
2024-04-11 01:17 PM
2024-06-21 01:00 PM
The observational data was polluted by a raft of other issues but resolved with the data in the above replies.