cancel
Showing results for 
Search instead for 
Did you mean: 

Is this MCU a fake of STM32F427VIT6?

DonFrana
Associate II

Hi,

 

can oneone help me to proof if the following MCU ist an original?

1)The print is easier to wipe off.
2)The revision number is missing or is not in the place described in the datasheet.

20240910_103406.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

It's new marking for LQFP100 package and it's the revision 4.

SofLit_1-1725964814428.png

SofLit_2-1725964997713.png

You can check by reading the revision from DBGMCU_IDCODE register.

SofLit_0-1725964714231.png

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

It's new marking for LQFP100 package and it's the revision 4.

SofLit_1-1725964814428.png

SofLit_2-1725964997713.png

You can check by reading the revision from DBGMCU_IDCODE register.

SofLit_0-1725964714231.png

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Thank you, this helped a lot!

And the register shows the correct value of 0x2003

 

The entire unique ID is:

DonFrana_0-1725970319684.png

@adresse 0xE0042000:
20036419 00000000 00001000

Is this the proof that this MCU is genuine?

It's a genuine MCU and  you read 0x2003 from the correct field. Why are you still not convinced?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Thanks.

 

It was not clear enough first.

 

Because:

1) the programmer shows 5/B in the blue area in the lower right corner  (I guess because 0x2003 stands for 4,5 or B)

2) The print is easy to wipe off (I have fotos if you want to see).

 

Thanks for your patience! -:)