2020-10-03 03:55 AM
2020-10-03 04:38 AM
Double or Single Precision?
Is that a 144-pin device? Guessing not
Floating point is done in software on CM0 and CM3 parts.
The CM4F has a single precision FPU that does some basic math functions, the remainder are handled in the library code.
Without some more specific reasoning, it sounds like you need a redesign.
2020-10-03 07:47 AM
There aren't any that are pin compatible. There are some that are close but have an additional VDD/VSS pair. See the "Pinout compatible" search feature in CubeMX.
2020-10-04 08:40 PM
2020-10-04 08:41 PM
Thanks you clive1
2020-10-04 08:41 PM
Thanks TDK