cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an API that allows you to send data greater than 8 bytes through the CAN communication protocol?

VNava.1
Associate III

I would like to build an application on an STM32 microcontroller (the one integrated in the NUCLEO-L432KC) that allows to transmit a message of 192 bytes or more if possible on CAN BUS.

At first, I was thinking of a mechanism that in the transmission phase allows me to divide the data into several 8-byte messages and then on the receiving side an inverse mechanism that allows me to reconstruct it. However, I came across an article that talks about ISO 15765-2 CAN-TP Protocol which is an international standard protocol used for sending more than 8-bytes of data over the CAN consecutive frames. Is there an ST API that implements this protocol?

Thank you in advance!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0