2021-12-07 12:44 PM
2021-12-07 1:11 PM
Yes, sounds possible
PWM Input mode typically allows for a CH1 or CH2 connected GPIO to reset CNT, and also latch CCR1/CCR2 with period and duty type counts.
Clock source should be able to associated with a handful of different TIM. Usually the RM covers the clock sourcing options, which tend to be limited/finite.
TIM2 / TIM5 are typically 32-bit counters
2021-12-07 1:19 PM
Thanks for the links and fast reply. I have been testing out multiple configurations using CubeMX and was not able to come up with one that would cover both requirements; individually was not an issue. I will review the linked material more deeply to see if it can work.