2019-06-25 07:23 AM
I would like to play with a dual core STM32F
2019-06-25 07:55 AM
There is a H745 Disco available. I do not know of a STM32F dual core.
2019-06-25 10:34 AM
Aha, STM32F != STM32H. I meant any multicore Discovery boards.
2019-06-25 11:16 AM
So You know that there are no STM32Fxxx dual core MCU, but are asking for "dual core board"? :)
2019-06-25 12:20 PM
The STM32H745I-DISCO board is available, have a handful here.
2019-06-25 12:51 PM
Thanks. Digikey does not list it yet. I'll have to wait a little bit more, I think. Ànd If I understood your post you linked correctly it is also a little immature.
I was asking any multicore board, no matter what's it's name or number of cores(as long it is more than one).
2019-06-25 02:11 PM
Well support is going to be a heavy lift.
The H747I-DISCO I have was built almost a year ago. The V-step silicon is now available and offering 480MHz M7, 240MHz M4
The NUCLEO-H743ZI2 is now available using the V-step silicon, and I expect the H745XI version to be available very soon. This board has the ST-LINK/V3
https://community.st.com/s/question/0D50X0000AyCT8KSQW/new-nucleoh743zi2-out
2019-06-25 03:03 PM
Interesting that the STM32H747 is revision V. The STM32H743 is revision V also.
Is that a coincidence or are the STM32H743 and STM32H747 the same die?