Is ther a possibility to search for MCU's by peripheral (SPI) speed?
Hello everybody!
This is my first post. I hope that i am on the right corner of this Q&A section.
For an application i need a MCU that is capable to run the SPI with a clock-frequency of at least 80MHz (Master transmit) and at least 50MHz (Master receive).
Now my problem is that all microcontroller i've used are limited in SPI-Speed (Master/Slave) far below this frequency.
Right now i've only found MCU's of the H7-series (randomly searched) that would achieve that SPI frequencies. But i think that the H7-series is mutch to powerful for my needings in all other aspects. I just need to write a few register via SPI with that high speed. Nothing more. well, and some timing for the register writing...not that effort.
Now my question is, if there is a way (on the homepage) to select MCU's via their peripheral speed/frequency (SPI in my case) so that i can pick a lower powered MCU that will also achieve this SPI frequency (like H7-series).
Or maybe some of you have already faced the same problem and could give me a tip where to search.
Thanky in advance