2020-12-08 11:36 PM
Your microcontroller STM32 L562RET6 claims NIST SP800-90B conformity.
Does this TRNG also fit the criteria of the functionality class PTG.2 in the document
"A proposal for: Functionality classes for random number generators" [1]
Is the TRNG also comform to the AIS31 standard?
Solved! Go to Solution.
2020-12-10 06:05 AM
Hello @SWans.1 ,
Welcome to the STM32 Community :smiling_face_with_smiling_eyes:
STM32L5 TRNG should be compliant to AIS31 PTG.2 class, but it has not been through the certification process yet.
Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this answer more quickly.
Imen
2020-12-10 06:05 AM
Hello @SWans.1 ,
Welcome to the STM32 Community :smiling_face_with_smiling_eyes:
STM32L5 TRNG should be compliant to AIS31 PTG.2 class, but it has not been through the certification process yet.
Please mark my answer as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this answer more quickly.
Imen
2020-12-10 07:39 AM
Thanks.