2021-03-10 12:45 AM
Announced over a year ago - I developed a product based on it and still no silicon
2021-03-10 1:29 AM
You have an open order for these or waiting for free stock at distribution? MoQ looks to be close to a 1000, with 26 week delivery.
What's the local sales rep telling you?
2021-03-10 9:33 AM
I've been monitoring the ST store ever since they announced and there has never been availability there or with any distributor. I'm only ever likely to need 3 or 400 so ordering 1000 is out of the question.
This is a very interesting chip, full LTDC and lots on internal RAM in a 64-pin package. The applications are endless if only the bloody thing existed!
2021-03-10 9:54 AM
Undoubtedly, however I suspect this is going into something specific (game device, end customer), or there is a specific log-jam into getting the die onto a 64-pin lead frame, along with all the other issues currently.
@STOne-32 any thoughts / projections on this? Sampling quantities?
2021-03-11 5:44 AM
Dear @Community member @Community member ,
We are very happy and delighted to see that the device is fitting your need {This is a very interesting chip, full LTDC and lots on internal RAM in a 64-pin package. The applications are endless if only the bloody thing existed!} as I see you are located in UK, we will contact you shortly to update regarding your wanted samples.
Ciao,
STOne-32
2021-03-11 9:10 AM
Thanks