cancel
Showing results for 
Search instead for 
Did you mean: 

Is the parameter 'ActiveFrameLength' and 'FrameLength' under the FrameInit significant when the SAI module is configured to operate in slave mode to receive data?

Jansunil
Associate II

I am trying to configure the SAI block in slave mode to receive a set of data. The Frame Sync signal and the data clock shall be provided from an external device. In a case where the active frame length and the frame length are to be decided by the master device, is it necessary that these parameters are configured during initialization of the block? If yes, is there a default value that is to be provided ?

0 REPLIES 0