cancel
Showing results for 
Search instead for 
Did you mean: 

Is the bootloader host code available in some form?

DavePfz
Associate II

I am working on a project where several STM32L0xx processors will be running under a Raspberry Pi 4+ system. The desire is to be able to use the SystemBootloader on these to be able to do firmware updates. I know that the documentation from ST is enough to beable to write such an application from scratch, but I was wondering if the core code might already be available.

Since this would be done as a sub-task to an application, no GUI or even CLI, it would be preferable of the code was in 'C', but anything would be a help to get started.

Thanks

2 REPLIES 2

Many people have written examples over the years.

A good example might be the Arduino firmware update tool for the MKR WAN 1300 that's on GitHub for sure.

This is a topic thats been covered here before.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Javier1
Principal

They dont discole the code.

But they do some efforts to give you opensource options

https://github.com/STMicroelectronics/stm32-mw-openbl

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero