2022-03-23 02:28 AM
With other MCUs I get an additional SDRAM 1 and SDRAM 2 option. Or is it only not available to configure in CubeMX and I should code it myself?
Thanks in advance.
2022-03-23 06:19 AM
The LQFP144 package lacks necessary pins for SDRAM and thus is unavailable for selection in CubeMX.
2022-03-23 07:49 AM
Hello,
Unfortunately, SDRAM feature is not available on LQFP144 packages in STM32H7xx products.
The update of STM32H755 datasheet is ongoing and a fix will be available like done in the latest version of STM32H753 datasheet (DS12117 Rev 😎 / Table 2.