cancel
Showing results for 
Search instead for 
Did you mean: 

Is five-volt tolerance guaranteed in Standby / Stop mode?

C.Ecke
Associate

I want to wake-up from standby mode on a STM32L422xx using PA2 (WKUP4) with pull-down enabled in PWR_PDCRA. Wake-up signal can go up to 5.25V at this pin.

Can this configuration cause any problems e.g. high current injection during wake-up phase?

Thanks in advance.

1 REPLY 1
TDK
Guru

No issues as long as it's powered appropriately.

0693W00000JOHiEQAX.png

If you feel a post has answered your question, please click "Accept as Solution".