Skip to main content
CWang.9
Visitor II
February 2, 2022
Question

Implement Cordic of Arctan2 through ADC and DMA

  • February 2, 2022
  • 0 replies
  • 871 views

I need to calculate angle value with input of sin/cos from ADC1/ADC2 channel by DMA way. As using the cordic of atan2 function,I think that two parameters of Y and X need to be written to pInBuff as like the key code below, is it correct?

 sCordicConfig.Function     = CORDIC_FUNCTION_PHASE;   /* atan2 function */

 sCordicConfig.Precision    = CORDIC_PRECISION_6CYCLES; /* max precision for q1.31 atan2 */

 sCordicConfig.Scale      = CORDIC_SCALE_0;      /* no scale */

 sCordicConfig.NbWrite     = CORDIC_NBWRITE_2;     /* Two input data: x and y */

 sCordicConfig.NbRead      = CORDIC_NBREAD_1;     /* One output data: atan2 */

 sCordicConfig.InSize      = CORDIC_INSIZE_32BITS;   /* q1.31 format for input data */

 sCordicConfig.OutSize     = CORDIC_OUTSIZE_32BITS;  /* q1.31 format for output data */

 if (HAL_CORDIC_Configure(&hcordic, &sCordicConfig) != HAL_OK)

 {

  /* Configuration Error */

  Error_Handler();

 }

HAL_ADC_Start_DMA(&hadc1, (uint32_t*) aSin, 1);

HAL_ADC_Start_DMA(&hadc2, (uint32_t*) aCos, 1);

aTan[0] = aSin[0];

aTan[1] = aCos[0];

HAL_CORDIC_Calculate_DMA(&hcordic, aTan, aArcTan2,1,CORDIC_DMA_DIR_IN_OUT)

This topic has been closed for replies.