cancel
Showing results for 
Search instead for 
Did you mean: 

Is DAC output on PA5 usable since it connects to L3GD20?

Bill Lewis
Associate III
Posted on March 07, 2013 at 20:46

On the STM32F3-Discovery, PA5 is connected to the L3GD20 gyro chip's SCLK input.

In general CMOS devices to not like having input hanging around voltages in between a good Low or High.  It causes excessive current consumption.

Will this be a problem, trying to use the DAC output on PA5?

-Bill

#dac
1 REPLY 1
raptorhal2
Lead
Posted on March 07, 2013 at 22:24

The other problem might be the limited DAC drive current.

Discovery boards are not expensive. If you don't need the gyro, cut the trace.

Cheers, Hal