Skip to main content
kaylee
Associate
Mar 7, 2013 4:02 PM UTC
Question

Issues with SPI 2 on STM32f100RB

Posted on March 07, 2013 at 17:02

I will need to use spi with a memory chip. But I currently can't get my spi to input data.

I am able to get it to output. I have a logic analyzer hooked up and it shows data is being outputed. When I do a loop back test it shows the data being delivered to the input pin PB14 but the micro does not seem to realize this.

I am thinking that I do not have the pin set up for input, but I have tried different configurations but nothing seems to work

This code sets up the spi, sends out data and is suppose to read it in

code:

void SPIInit (void)

{

* regRCC_APB2ENR = 0x9; //turn on gpiob and afio

* regRCC_APB1ENR = 0x4000; // turn on spi 2

* regGPIOB_CRH = 0xB4B34B44; //this is where i might be having issues

* regSPI_CR1 = 0x334;

//* regSPI_CR2 = 0x04;

* regSPI_CR2 = 0x00;

* regSPI_CR1 |= 0x0040;

}

void SendOne()

{

char data;

*regGPIOB_BSRR = 0x00001000;//CS high (set) PB12

while ((* regSPI_SR & 0x02 )!= 0x02){;} // when transmit buffer is empty send data

*regSPI_DR = 0x9; // send enable to memory chip EWEN

//*regSPI_DR = 'a'; // send enable to memory chip EWEN

//edited it below as it was 0x2 and it was suppose to be 0x1

while ((* regSPI_SR & 0x000001 )!= 0x01){;} // when receive buffer not empty read data, program getting stuck here

data = * regSPI_DR; //reading clears flags

//*regGPIOB_BSRR = 0x00001000; //reset chip select low

}

spi

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Mar 7, 2013 4:40 PM UTC
Posted on March 07, 2013 at 17:40

> while ((* regSPI_SR & 0x000002 )!= 0x02){;} // when recieve buffer not empty read data, program getting stuck here

No wonder: this is not proper mask to get the ''receive buffer not empty'' flag; it's bit 0 of SPI_SR register.

It's perhaps not a good idea to use ''magic values''. The STM32F0xx_StdPeriph_Lib_V1.0.0\Libraries\CMSIS\Device\ST\STM32F0xx\Include\stm32f0xx.h header is there for a reason.

JW

[EDIT] I take back the ''no wonder''. While the incorrect bit is read and checked indeed, the program should go on with incorrect data read from SPI_DR, as TXE should be set by hardware at the beginning of transmission. I don't understand why it is stuck.

kaylee
kayleeAuthor
Associate
Mar 7, 2013 6:25 PM UTC
Posted on March 07, 2013 at 19:25

Thank you for noticing that.

I did have 0x01 previously but changed it while testing and watching the register values.

I will edit it to the appropriate value