cancel
Showing results for 
Search instead for 
Did you mean: 

Inverted polarity COMParator

ADedk.1
Associate

Hello. I use STM32G474VET6.

I want to use the comparator output as an external event for the timer. The output of the comparator (event) must be inverse (the POL bit is set in the COMP_CxCSR register). However, according to the logic of work, I see that the inverter does not affect the polarity of the event. Are my assumptions true or am I doing something wrong?

1 ACCEPTED SOLUTION

Accepted Solutions
ADedk.1
Associate

I downloaded the version 3 manual. There are no more questions.

View solution in original post

2 REPLIES 2
ADedk.1
Associate

I downloaded the version 3 manual. There are no more questions.

Thanks for coming back with the solution.

Please select your post as Best so that the thread is marked as solved.

JW