2024-08-01 9:46 PM
Hello ST Community,
I am currently attempting to establish communication between two STM32U585 boards using the Serial Peripheral Interface (SPI) protocol.
Issue Encountered: Data is not being received.
The transmission from one of the STM32U585 boards is functioning correctly, as confirmed by testing with a logic analyzer. However, the issue lies with the reception on the other STM32U585 board. We have tried both the polling method (which resulted in a timeout error) and the interrupt method (where no callback was received) for SPI communication.
I would appreciate any guidance or suggestions to resolve this issue.
Thanking you,
Nirupama
2024-08-02 12:01 AM
2024-08-02 4:27 AM
Ensure slave is ready to receive prior to the master sending a frame. Ensure pins are connected appropriately. Show your code.