interrupt call back response time
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 8:12 AM
Using a stm32h7
From what I gather this 1.5 responce tie is normal. Is there a trick or two I can use to speed this up? Can I move the callback location in memory? I'd like to get this much closer to a a few ticks.
- Labels:
-
Interrupt
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 9:12 AM
maybe better is show code. Normal latency for EXTI is in reference manual .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 9:23 AM
Code is generate by ioc, it should all be standard. I'm using the HAL
pin config was generated with
/*Configure GPIO pin : PF14 */
GPIO_InitStruct.Pin = GPIO_PIN_14;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
call back is just
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
Test_Execut_start_GPIOG4; //used for debug trace
Test_Execut_stop_GPIOG4;
if (GPIO_Pin == GPIO_PIN_14)
{
//do code
}
}
but from the time the int fires to the code its nearly 1.5us.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 10:30 AM
Several factors will affect the timing. Measure the latency not by a GPIO (which adds latency) but by issuing a SEV instruction and measuring a pulse at any pin configured as EVENTOUT. You may add 2 SEV's, one at the beginning of the native IRQ handler void EXTI15_10_IRQHandler(void) (in stm32h7xx_it.c) and a second one in the HAL callback to measure the HAL overhead. Also check that the IRQ handler is compiled with high optimization level such that the function prolog and epilog code is tiny. Check this in disassembly by setting a breakpoint at the handler. And, yes, flash latency may also be an issue which can be eliminated by moving the handler code to SRAM. Disclaimer: not tested on H7 but smaller chips.
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 11:17 AM
Are all the EXTI vectors going to be regrouped by hal into a unique callback? If yes, hardly speed optimized....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-06 12:35 PM
HAL_GPIO_EXTI_Callback is not the direct callback function. The callback is EXTIx_IRQHandler, which calls HAL_EXTI_IRQHandler, which calls HAL_GPIO_EXTI_Callback. 1.5us to get through that code, plus about 12 ticks for the IRQ itself to fire seems about right.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-07 6:27 AM
thx guys this is exactly what I was looking for
void EXTI15_10_IRQHandler(void)
{
/* USER CODE BEGIN EXTI15_10_IRQn 0 */
/* USER CODE END EXTI15_10_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_14);
/* USER CODE BEGIN EXTI15_10_IRQn 1 */
/* USER CODE END EXTI15_10_IRQn 1 */
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-07 6:51 AM
its saved me a whopping 126 ns
void EXTI15_10_IRQHandler(void)
{
Test_Execut_start_GPIOG4;
/* USER CODE BEGIN EXTI15_10_IRQn 0 */
/* USER CODE END EXTI15_10_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_14);
/* USER CODE BEGIN EXTI15_10_IRQn 1 */
Test_Execut_stop_GPIOG4;
/* USER CODE END EXTI15_10_IRQn 1 */
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-07 7:25 AM
ok unlesss 1us is not enough time for the st to re arm the irq I think I the issue is code related. it seem to fire correctly the first time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-12-07 8:07 AM
For 12 and 180MHz for example 66,6ns plus interrupt init instruction cycles...