2022-07-18 3:15 AM
In STM32F103xx manual, Synchronous non-multiplexed PSRAM write timings gragh (76page, Figure 31) is wrong?? This is same Synchronous multiplexed PSRAM read timings(Figure 28).
Please let me know if the manual is wrong or if I'm wrong
2022-07-18 4:07 AM
Do you mean Datasheet? For which STM32 exactly?
JW
2022-07-18 4:28 AM
Welcome, @SHa.3, to the community!
correct and sorry for the mistake, the data sheet is wrong and shows the multiplexed timings in figures 28 and 31 of the data sheet DS5792 of the STM32F103xC, STM32F103xD, STM32F103_E.
A correct timing can be seen in figures 26 and 28 of the data sheet DS6558 of the STM32F103xF, STM32F103xG.
@Sara BEN HADJ YAHYA
Regards
/Peter
2022-07-18 1:41 PM
Hi Peter,
> wrong and shows the multiplexed timings in figures 28 and 31 of the data sheet DS5792 of
> the STM32F103xC, STM32F103xD, STM32F103_E.
> A correct timing can be seen in figures 26 and 28 of the data sheet DS6558 of the
> STM32F103xF, STM32F103xG.
I freshly downloaded the DS from links you've provided and fail to see the difference between fig.28/'C'D'E and fig.26/'F'G:
whereas fig.31/'C'D'E and fig.28/'F'G are completely different. However, fig.31/'C'D'E and fig.29/'F'G are again identical, and both wrong (or their caption is wrong - I now don't try to understand the "logic" behind FSMC's "modes" - I would like to, but it's a mess and ST never cared enough to produce the dozen of appnotes needed to clean it up):
Jan
@Peter BENSCH
[EDIT] PS. Where is DS5792 and DS6558 from? Why can't I see these numbers in the DS themselves?
2022-07-18 6:00 PM
2022-07-18 11:48 PM
Well, the data sheets still have some inconsistencies that apparently have not been noticed so far, in this respect we would also like to thank you for reading them attentively.
As far as the document numbers are concerned, you can find them as data sheet numbers on the respective product website, e.g. here for the 'CDE, sometimes they are also on the respective data sheet in the footer. In addition, you can download the entire current documentation (AN, DB, DS, ES, PM, RM, UM) of the STM32 into your repository, where the PDFs with these document numbers (DS5792, RM0008, etc) are stored:
Regards
/Peter
2022-07-19 2:02 AM