2019-04-24 08:17 AM
In Atollic, I imported the GPIO example (Blink) which compiled.
Trying to Run or Debug in Atollic an IP address is requested. But the board is connected via USB. I have not found no option to flas via USB.
2019-04-25 02:05 AM
Hello,
STM32CubeProgrammer is an all-in-one multi-OS software tool for programming STM32 microcontrollers, allowing to flash STM32 devices through the SWD/JTAG debug interface and via the UAR/USB bootloader interface.
Regards,
Imen