cancel
Showing results for 
Search instead for 
Did you mean: 

Im using stm32F373c8t6 MCU, i want to interface i2c2 peripheral with MCP7904N(EEPROM IC). i have generated configure file from cubeMx .. This board is tested ok.

Asing.1
Associate II

when i write or read it show hal_ok..

if(HAL_I2C_Mem_Write(&hi2c2, 0xA0, 0, 1, eeprom_tx_buff, 1,15) == HAL_OK)

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);

It shows hal_ok .

if(HAL_I2C_Mem_Read(&hi2c2, 0xA1, 0, 1, eeprom_tx_buff, 1,15) == HAL_OK)

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);

but when i read eeprom_tx_buff[0] it shows 0xff..

Please help me to find the solution

0 REPLIES 0