cancel
Showing results for 
Search instead for 
Did you mean: 

Im facing CAN transmit error,HAL_CAN_ERROR_TX_TERR0 (0x00001000U) /*!< TxMailbox 0 transmit failure due to transmit error */. Can anyone guide me how to resolve this or what is the reason for this error. Im using a NUCLEO-F767ZI board.

SG.11
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @SG.11​ and welcome to the Community :)

I advise you to refer to the CAN examples available within STM32CubF7 MCU package.

Have a look at this post, this may help you.

It would be better to provide more details about your project and configuration, this will help Community users to answer you.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Karl Yamashita
Principal

Show us snippets of the code you wrote

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source