2018-09-18 11:40 PM
2019-10-28 9:07 PM
Hello to all! I was wondering if you managed to get the H7 going on the 7 version of IAR? I have been trying all kind of things and so far everything I tried end up with a "Failed to load flash loader: ...FlashSTM32H753_BANK1.flash".
Is there some proper procedure documented on how to get this working?
Also is there anyway possible to get the H7_V1.3.0 cube package to get this EWARM_v7_STM32H750xx_Support.zip file? As, as of this day the cube has been updated and the new versions hold the v8 of the EWARM_v8_STM32H750xx_Support.zip. Or it doesnt matter which version it says and it should work for iar 7?
Thanks in advance for any advice.
Regards,
Konstantin
2019-10-28 9:26 PM
The EWARM 7 files
https://drive.google.com/open?id=1V94vdMga3cJHVIlUleMv4OUqcz_PtA5-
The whole CubeH7 1.3.0
https://drive.google.com/open?id=1s73-yuG0WwdNhz8JEMdzx1rFmqeM21SK
2019-10-28 9:39 PM
This was fast! Thanks so much!
Would it be a better idea to reinstall IAR clean if I applied the EWARM_v8 file to the 7.8 iar folder?
Thanks again!
Konstantin
2019-10-28 10:08 PM
Yes! This worked straightforward!
Appreciate it once more, my friend!