2019-10-29 12:42 AM
After doing debugging i have found that the error code is set by DMA config function :
HAL_StatusTypeDef HAL_DMA_Start_IT(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength)
{
.
.
.
.
.
else
{
/* Process unlocked */
__HAL_UNLOCK(hdma);
/* Set the error code to busy */
hdma->ErrorCode = HAL_DMA_ERROR_BUSY; //< this line is setting error code >
/* Return error status */
status = HAL_ERROR;
}
return status;
}here are my configs for ADC1 and ADC2:
hadc1.Instance = ADC1;
if (HAL_ADC_DeInit(&hadc1) != HAL_OK)
{
/* ADC de-initialization Error */
Error_Handler();
}
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/
hadc1.Init.Resolution = ADC_RESOLUTION_16B; /* 16-bit resolution for converted data */
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */
hadc1.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */
hadc1.Init.ContinuousConvMode = ENABLE; /* Continuous mode enabled (automatic conversion restart after each conversion) */
hadc1.Init.NbrOfConversion = 3; /* Parameter discarded because sequencer is disabled */
hadc1.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */
//hadc1.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */
hadc1.Init.OversamplingMode = DISABLE; /* No oversampling */
/* Initialize ADC peripheral according to the passed parameters */
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/* ### - 2 - Start calibration ############################################ */
if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
/* ### - 3 - Channel configuration ######################################## */
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_15;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
/*
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
*/
/* ### - 4 - Start conversion in DMA mode ################################# */
if (HAL_ADC_Start_DMA(&hadc1,
(uint32_t *)aADCxConvertedData,
ADC_CONVERTED_DATA_BUFFER_SIZE
) != HAL_OK)
{
Error_Handler();
}
/**************************************ADC3*********************************************/
hadc3.Instance = ADC3;
if (HAL_ADC_DeInit(&hadc3) != HAL_OK)
{
/* ADC de-initialization Error */
Error_Handler();
}
hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/
hadc3.Init.Resolution = ADC_RESOLUTION_12B; /* 16-bit resolution for converted data */
hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */
hadc3.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */
hadc3.Init.ContinuousConvMode = ENABLE; /* Continuous mode enabled (automatic conversion restart after each conversion) */
hadc3.Init.NbrOfConversion = 3; /* Parameter discarded because sequencer is disabled */
hadc3.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */
//AdcHandle.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */
hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */
hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */
hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */
hadc3.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */
hadc3.Init.OversamplingMode = DISABLE; /* No oversampling */
/* Initialize ADC peripheral according to the passed parameters */
if (HAL_ADC_Init(&hadc3) != HAL_OK)
{
Error_Handler();
}
/* ### - 2 - Start calibration ############################################ */
if (HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
/* ### - 3 - Channel configuration ######################################## */
/** Configure Regular Channel
*/
sConfig3.Channel = ADC_CHANNEL_9;
sConfig3.Rank = ADC_REGULAR_RANK_1;
sConfig3.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig3.SingleDiff = ADC_SINGLE_ENDED;
sConfig3.OffsetNumber = ADC_OFFSET_NONE;
sConfig3.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig3) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig3.Channel = ADC_CHANNEL_4;
sConfig3.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig3) != HAL_OK)
{
Error_Handler();
}
sConfig3.Channel = ADC_CHANNEL_8;
sConfig3.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig3) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
/*
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)
{
Error_Handler();
}
*/
/* ### - 4 - Start conversion in DMA mode ################################# */
if (HAL_ADC_Start_DMA(&hadc3,
(uint32_t *)aADC3ConvertedData,
ADC_CONVERTED_DATA_BUFFER_SIZE
) != HAL_OK)
{
Error_Handler();
}
2019-10-29 12:43 AM
here is the HAL_Msp_Init() function:
void HAL_ADC_MspInit(ADC_HandleTypeDef *hadc)
{
GPIO_InitTypeDef GPIO_InitStruct;
static DMA_HandleTypeDef DmaHandle;
static DMA_HandleTypeDef hdma_adc3;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO clock ****************************************/
/*##- 3- Configure DMA #####################################################*/
/*********************** Configure DMA parameters ***************************/
if(hadc->Instance == ADC1){
__HAL_RCC_ADC_CONFIG(RCC_ADCCLKSOURCE_CLKP);
ADCx_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/* ADC Channel GPIO pin configuration */
GPIO_InitStruct.Pin = ADCx_CHANNEL_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(ADCx_CHANNEL_GPIO_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
DMAx_CHANNELx_CLK_ENABLE();
DmaHandle.Instance = DMA1_Stream1;
DmaHandle.Init.Request = DMA_REQUEST_ADC1;
DmaHandle.Init.Direction = DMA_PERIPH_TO_MEMORY;
DmaHandle.Init.PeriphInc = DMA_PINC_DISABLE;
DmaHandle.Init.MemInc = DMA_MINC_ENABLE;
DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
DmaHandle.Init.Mode = DMA_CIRCULAR;
DmaHandle.Init.Priority = DMA_PRIORITY_MEDIUM;
DmaHandle.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
/* Deinitialize & Initialize the DMA for new transfer */
HAL_DMA_DeInit(&DmaHandle);
HAL_DMA_Init(&DmaHandle);
/* Associate the DMA handle */
__HAL_LINKDMA(hadc, DMA_Handle, DmaHandle);
/* NVIC configuration for DMA Input data interrupt */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
}
if(hadc->Instance == ADC3){
__HAL_RCC_GPIOF_CLK_ENABLE();
/* ADC Periph clock enable */
__HAL_RCC_ADC3_CLK_ENABLE();
/* ADC Periph interface clock configuration */
/* Enable DMA clock */
__HAL_RCC_DMA2_CLK_ENABLE();
/*##- 2- Configure peripheral GPIO #########################################*/
GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_4 | GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
hdma_adc3.Instance = DMA1_Stream2;
hdma_adc3.Init.Request = DMA_REQUEST_ADC3;
hdma_adc3.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc3.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc3.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc3.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc3.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc3.Init.Mode = DMA_CIRCULAR;
hdma_adc3.Init.Priority = DMA_PRIORITY_HIGH;
hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
/*
hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_adc3.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_3QUARTERSFULL;
*/
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc3);
HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
}
}