2016-12-05 8:45 AM
Hi folks,
my application crashes occasionally with the above mentioned firmware package when data is transmitted to I2C devices.
The crash is caused by following code in HAL_I2C_Master_Transmit:
while(hi2c->XferSize > 0U)
{
/* Wait until TXE flag is set */
if(I2C_WaitOnTXEFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
...
}
/* Write data to DR */
hi2c->Instance->DR = (*hi2c->pBuffPtr++);
hi2c->XferCount--;
hi2c->
XferSize
--;if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (
Size
!= 0U)){
You can get here when
I2C_FLAG_BTF
is set due to delay (interrupt) andXferSize
== 0 because the wrong var (Size
) is checked. This results inXferSize
wrapping around to 0xffff. The transmit loops continues and usually thepBuffPtr
runs beyond bounds causing a bus error./* Write data to DR */
hi2c->Instance->DR = (*hi2c->pBuffPtr++);
hi2c->XferCount--;
hi2c->XferSize--;
}
This code fragment can be found several times in stm32f2xx_hal_i2c.c.
I temporarily went back to Rev 1.3.0.
Christian
2016-12-06 2:29 AM
Hi
backeberg.christian
,Thank you for the feedback and contribution. I send internally your request for check.
-Walid FTITI-
2017-10-18 7:58 AM
Hi Walid,
recently I noticed an update of stm32f2xx_hal_i2c.c to revision 1.6.
I checked it against the above mentioned bug.
It seems that the bug has not being fixed in all places were it can occur.
In HAL_I2C_Slave_Receive() at Line 1142 the old code can be found.
Christian
2017-10-18 9:18 AM
Hi
backeberg.christian
,Thanks for highlighting this again, this will be reviewed and fixed.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-01 8:19 AM
Sorry, but the above mentioned bug is still not fixed in Rev 1.7.0.
Line 1140:
if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (Size != 0))
should be:
if((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BTF) == SET) && (hi2c->XferSize != 0))
Greetings - Christian