cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know how to configure RCC on my evaluation Board STM32L552E-EV.

DYann.1
Senior

I connect my I2C but when I connect an oscilloscope I have nothing on the clock signal. So probably I misconfigured my clock. Could you give me the information? Thanks in advance.

In this picture below I've a warning, do you know how to remove this warning please ?

0693W00000aI9LSQA0.pngThank you for your helps.

Regards

Yann DO

27 REPLIES 27
DYann.1
Senior

It's very strange when I come back to the '.ioc' I have a error and I selected resolve the error automatically. Now I have this configuration :

0693W00000aINGsQAO.pngNormally the value is 8 but now it's 16. So I cant try again.

DYann.1
Senior

I have a warning :

0693W00000aINNhQAO.pngImplicit declaration what does it means ?

But it's not very important, I can working. Now I have the clock on the SCL (just to have pull-up inside no pull-up).

But I have always the same error

DYann.1
Senior

Hi,

Sorry I have another error :

0693W00000aINBmQAO.pngbuff[0] had to make a shift. But I have always the same error.

Did you add the prototypes?

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.

Yes I have developed prototypes but the error comes from SysTick as I sent you an email. How to configure the SysTick with my evaluation Board STM32L552E-EV ? Just to check if my board still works.

Explain your error.

And use the code snippet icon to add code instead of images. Makes it easier to copy code.

0693W00000aIcMZQA0.png

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.

You can use this I2C example. It's the same STM32L5 family and not tied to a specific development board.

0693W00000aIcOGQA0.png

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.
DYann.1
Senior

Hi,

As I say before I modify my code to check the SysTick function

int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
/* Configure the peripherals common clocks */
  PeriphCommonClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_I2C1_Init();
  MX_SAI1_Init();
  /* USER CODE BEGIN 2 */
 
  HAL_Delay(50);
  HAL_Delay(50);
  // SGTL5000_init();
  // set_volume(0);
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

And inside my function Hal_Delay (50), I'm always stuck in this line

__weak void HAL_Delay(uint32_t Delay)
{
  uint32_t tickstart = HAL_GetTick();
  uint32_t wait = Delay;
 
  /* Add a period to guaranty minimum wait */
  if (wait < HAL_MAX_DELAY)
  {
    wait += (uint32_t)uwTickFreq;
  }
 
  while ((HAL_GetTick() - tickstart) < wait)
  {
  }
}

And inside this function, it never returns to the calling function

__weak uint32_t HAL_GetTick(void)
{
  return uwTick;
}

 Do you know how to configure the SysTick of my evaluation board STM32L552E-EV ?