2019-09-25 12:09 AM
I have generated the driver codes using STM32Cube MX. I am attaching wth this the source codes of both master(main)and slave (main_F3) microcontrollers.
Could you help me with this
2019-09-26 7:54 AM
Are pins initialized?
Can you do a scope trace to see if signal is being sent?
Is chip select pin behaving correctly?
Didn't look at the code but that’s where I’d start.