cancel
Showing results for 
Search instead for 
Did you mean: 

Source code included in STSW-STM32080 package for STM32 DfuSe utility

Central SUPPORT
Senior II

Product folder on st.com and databrief says "The STSW-STM32080 package contains all binaries and source code for DfuSe USB device firmware upgrade (DFU) software, including the demonstration, debugging GUIs, and protocol layers." Same is also mentioned in the readme.txt in the package.

I downloaded the package but could not find the sources in downloaded file. So, where are they?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

Please note that for new STM32 products, it is recommended to use STM32CubeProgrammer.

View solution in original post

2 REPLIES 2
Central SUPPORT
Senior II
  1. After download please launch DfuSe_Demo_V3.0.6_Setup.exe
  2. Once this installation has been done, all sources are available at this location (default setting): C:\Program Files (x86)\STMicroelectronics\Software\DfuSe v3.0.6\Sources

Central SUPPORT
Senior II

Please note that for new STM32 products, it is recommended to use STM32CubeProgrammer.